SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
Figure 12-54 shows an overview of the MLBSS software and data flow when transmitting.
Figure 12-54 MLBSS Software and Data Tx Flow OverviewThe MLBSS data Tx flow is defined in the following way:
Figure 12-55 shows an overview of the MLBSS software and data flow when receiving.
Figure 12-55 MLBSS Software and Data Rx Flow OverviewThe MLBSS data Rx flow is defined in the following way:
Steps 1 and 2 from Figure 12-54 and Figure 12-55 are done by software. For more information see Section 12.1.4.4.1.1.1, Channel Initialization.
Steps 3-5 from Figure 12-54 and Figure 12-55 are handled by MLBSS internal hardware.
The top-level software tasks that the application must perform, can be placed in two categories:
For more information about channel initialization, see Section 12.1.4.4.1.1.1, Channel Initialization.
For more information about channel servicing, see Section 12.1.4.4.2.1, Channel Servicing.