SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The sequence for using SDMA is shown in Figure 12-36.
Figure 12-225 Transaction Control with Data Transfer Using DAT Line Sequence (Using SDMA)(1) Data location of system memory is set to the SDMA System Address register if MMCSD0_HOST_CONTROL2[12] HOST_VER40_ENA = 0 or set to the MMCSD0_ADMA_SYS_ADDRESS register if MMCSD0_HOST_CONTROL2[12] HOST_VER40_ENA = 1.
(2) Set the value corresponding to the executed data byte length of one block in the MMCSD0_BLOCK_SIZE register.
(3) Set the value corresponding to the executed data block count in the MMCSD0_BLOCK_COUNT register in accordance with Determination of Transfer Type.
(4) Set the argument value to the Argument register (MMCSD0_ARGUMENT1_LO and MMCSD0_ARGUMENT1_HI).
(5) Set the value to the MMCSD0_TRANSFER_MODE register. The Host Driver determines Multi/Single Block Select, Block Count Enable, Data Transfer Direction, Auto CMD12 Enable and DMA Enable in the MMCSD0_TRANSFER_MODE register. Multi/Single Block Select and Block Count Enable are determined according to Determination of Transfer Type. If response check is enabled (MMCSD0_TRANSFER_MODE[7] RESP_ERR_CHK_ENA = 1), set MMCSD0_TRANSFER_MODE[8] RESP_INTR_DIS bit to 1 and select Response Type R1/R5.
(6) Set the value to the MMCSD0_COMMAND register.
Note: When writing to the upper byte [3] of the MMCSD0_COMMAND register, the SD command is issued and SDMA is started.
(7) If response check is enabled, go to stop (10) else wait for the Command Complete Interrupt (MMCSD0_NORMAL_INTR_STS[0] CMD_COMPLETE bit).
(8) Write 1 to the MMCSD0_NORMAL_INTR_STS[0] CMD_COMPLETE bit to clear this bit.
(9) Read Response register (MMCSD0_RESPONSE_0 - MMCSD0_RESPONSE_7) and get necessary information of the issued command.
(10) Wait for the Transfer Complete Interrupt (MMCSD0_NORMAL_INTR_STS_ENA[1] XFER_COMPLETE) and DMA Interrupt (MMCSD0_NORMAL_INTR_STS_ENA[3] DMA_INTERRUPT).
(11) If MMCSD0_NORMAL_INTR_STS_ENA[1] XFER_COMPLETE bit is set to 1, go to Step (14) else if MMCSD0_NORMAL_INTR_STS_ENA[3] DMA_INTERRUPT bit is set to 1, go to Step (12). The MMCSD0_NORMAL_INTR_STS_ENA[1] XFER_COMPLETE bit is higher priority than the MMCSD0_NORMAL_INTR_STS_ENA[3] DMA_INTERRUPT bit.
(12) Write 1 to the MMCSD0_NORMAL_INTR_STS_ENA[3] DMA_INTERRUPT bit to clear this bit.
(13) Set the next system address of the next data position to the System Address register (MMCSD0_ADMA_SYS_ADDRESS) and go to Step (10).
(14) Write 1 to the MMCSD0_NORMAL_INTR_STS_ENA[1] XFER_COMPLETE bit and MMCSD0_NORMAL_INTR_STS_ENA[3] DMA_INTERRUPT bit to clear this bit.
Note: Step (2) and Step (3) can be executed simultaneously. Step (5) and Step (6) can also be executed simultaneously.