SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
In the OSPI boot mode, the ROM Code initializes the OSPI module and the image is read from the OSPI flash connected to the selected chip-select. If the image fails to be read correctly from offset 0x0 of the flash memory, the ROM will attempt to obtain the image at offset 0x400000. This is the only redundant image location supported by the ROM. See OSPI Boot Device Configuration for OSPI port settings.
A detailed summary of the OSPI boot parameter table and the boot configuration definitions are listed in OSPI Boot Parameter Table.