The 22-bit fetch value is made up of the 14-bit fetch count and the 8-bit fetch allow.
The fetch time indicates the number of wireside clocks that the fetch allow will be active.
The fetch count is in Ethernet wireside clocks
which is bytes in Gigabit mode
(CPSW3_CPSW_NU_CPSW_NU_ETH_MAC_i_PN_MAC_CONTROL_REG[7]
GIG = 1h) and nibbles in 10/100Mbps mode.
When a fetch allow bit is set, the corresponding priority is enabled to begin packet transmission on an allowed priority subject to rate limiting. The actual packet transmission on the wire may carry over into the next fetch count and is the reason for the wire clear time in the fetch zero allow.
When a fetch allow bit is cleared, the
corresponding priority is not enabled to transmit for the fetch count
time.
A non-zero fetch allow value with a non-zero fetch count causes the fetch allow value to be applied for the fetch count number of wireside clocks.
A zero fetch count causes the associated fetch allow to be held for the duration of the cycle (until the next cycle start).
A zero fetch allow with a non-zero fetch count is intended to clear the wire for a scheduled (timed) express packet in the next fetch. A zero fetch allow indicates that no packet can be started for transmission for the associated fetch count. The associated fetch count must be sufficient to guarantee that the wire is cleared given that a packet on an allowed priority in the previous fetch could have been started on the previous clock and that there is hardware latency in the clear time. The timed packet should be sent on a priority that is enabled in the next fetch but disabled in the current zero allow fetch. The fetch allow previous to a zero allow should have only prempt priorities enabled or only express priorities enabled but not both.
The number of clocks required to clear the wire varies depending Ethernet wire speed and on whether express or prempt priorities were allowed in the previous fetch command.