SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
AVBTP assumes that AVB node media clocks are clocked by free-running oscillators. It is also assumed that the node's internal concept of wall clock time has been synchronized to the PTP Grandcontroller. AVBTP media clock sources embed "AVBTP Presentation Timestamps" in AVBTP streaming packets. Figure 12-155 illustrates the relationship between PTP network time and AVBTP Presentation Timestamps.
Figure 12-155 Cross Time Stamping and Presentation Timestamps