SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The Destination Command FIFO stores VBUSM transaction commands which are output from the MSM as modified versions of transactions that were popped from the Source Command FIFO. The Destination command FIFO allocates a new command ID for each read or write command that is pushed to the FIFO. Read IDs are allocated from a scoreboard maintained in the Destination Read Data FIFO. Write IDs are allocated from a scoreboard maintained in the Destination Write Status FIFO. When a new command is allocated, the Destination Command FIFO also pushes the original cid and crouteid values from the source side transaction into a scoreboard in either the Destination Read Data or Destination Write Status FIFOs depending on the applicable transaction direction. The read interface of the Destination Command FIFO directly drives commands onto the destination VBUSM command interface.