SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
Figure 12-219 and Figure 12-220 shows initialization and card identification sequence for the Standard Capacity SD Memory Card (SDSC), the High Capacity SD Memory Card (SDHC) and the Extended Capacity SD Memory Card (SDXC) that was based on the Physical Layer Version 3.01. Refer to the latest sequence.
Figure 12-219 Card Initialization and Identification (1)
Figure 12-220 Card Initialization and Identification (2)(1) SD Bus mode is selected by CMD0 (Keep Pin 1 to high during CMD0 execution).
(2) New CMD8 shall be issued after CMD0 to support High Capacity SD Memory Card.
(3) Voltage check command enables the Hosts to support future low voltage specification. However, at this time, only one voltage is defined. Legacy cards and Not SD cards do not respond to CMD8. In this case, set F8 to 0 (F8 is CMD8 valid flag used in step (11)) and go to Step (5). Only Version 2.00 or higher cards can respond to CMD8. The host needs to check whether CRC of the response is valid and whether VHS and check pattern in the argument are equal to VCA and check pattern in the response. Passing all these checks results in CMD8 response OK. In this case, set F8 to 1 and go to step (5). If one of the checks is failed, go to step (4).
(4) Initialization is stopped by CMD8 fails. The Host Driver should retry step (1) to (3) one more time (this is not described in the figure).
(5) SDIO OCR is available by issuing CMD5 with setting voltage window (bit 23 to 0) in the argument to 0. SDIO initialization is not started.
(6) No response means the card does not have SDIO function. Set SDIO flag to 0 and go to step (11). If the card responds to CMD5 and the response is OK, go to step (7). If the response is error, set SDIO flag to 0 and go to step (10). SDIO flag indicates whether SDIO functions are initialized or not.
(7) The SDIO portion starts initialization by CMD5 with setting the supply voltage to the voltage window. UHS-I supported host sets S18R to 1. If the supplied voltage is not matched with voltage window of card, the card goes into inactive state and does not return the response.
(8) If no response or error response is receive, set SDIO flag to 0 and go to step (10). If good response is received, go to step (9).
(9) Check busy status in the response. If busy is released, set SDIO flag to 1 and go to step (10). Repeat from step (7) while busy is indicated. Detecting timeout of 1 second exits the loop. In this case, set SDIO flag to 0 and go to step (10).
(10) Good response in this step means that all responses received at (6) and (8) are valid. When response is good, MP (memory present) flag in the response can be checked. If the response valid and MP = 0, go to step (28). Otherwise, go to step (11).
(11) Check F8 flag set in step (3). If CMD8 is executed correctly (F8 = 1), go to step (19). Otherwise, go to step (12).
(12) OCR is available by issuing ACMD41 with the voltage window (bit 23 to 0) in the argument is set to 0. Memory initialization is not started. The response of CMD55 (ACMD41) may indicate illegal command error due to some SD cards do not recognized CMD8. The Host Driver should ignore this error or issue CMD0 before ACMD41 to clear this error status.
(13) If response of CMD55 is not received, the card is not SD cards and goes to (17). If the card responds to CMD55, it may also respond to CMD41. If the responses of ACMD41 are OK, go to Step (14). Otherwise, go to step (28). Locked card can be detected by the card status in the response of CMD55.
(14) The memory portion starts initialization by Issuing ACMD41 with setting the supply voltage to the voltage window. If the supplied voltage is not matched with voltage window of card, the card goes into inactive state and does not return the response.
(15) If no response or error response is received, go to step (28). If good response is received, go to step (16).
(16) Check busy status in the response. If busy is released, go to step (18). Repeat from step (14) while busy is indicated. The interval of ACMD41 shall be less than 50 ms. Detecting timeout of 1 second exits the loop and go to step (28).
(17) The host recognizes that the card is not SD memory card and quits SD card initialization.
(18) The host recognizes that the card is Version 1.xx Standard Capacity SD Memory Card. Go to Step (30).
(19) OCR is available by issuing ACMD41 with setting the voltage window (bit 23 to 0) in the argument is set to 0. Memory initialization is not started. Setting of HCS does not affect this operation.
(20) If the card responds to CMD55, it may also respond to CMD41. If the responses of ACMD41 are OK, go to Step (21). Otherwise, go to step (28). Locked card can be detected by the card status in the response of CMD55.
(21) The memory portion starts initialization by Issuing ACMD41 with setting the supply voltage to the voltage window. UHS-I supported host sets S18R to1. If the host can supply more than 150mA, XPC is set to 1. HCS in the argument is set to 1, which indicates supporting High Capacity Memory Card. If the supplied voltage is not matched with voltage window of card, the card goes into inactive state and does not return the response.
(22) If no response or error response is received, go to step (28). If good response is received, go to step (23).
(23) Check busy status in the response. If busy is released, go to step (24). Repeat from step (21) while busy is indicated. The interval of ACMD41 shall be less than 50 ms. Detecting timeout of 1 second exits the loop and go to step (28).
(24) CCS in the response is valid after busy is released. If CCS = 0, it indicates the Standard Capacity SD Memory Card and go to step (25). If CCS = 1, it indicates the High Capacity SD Memory Card or Extended Capacity Memory Card and go to Step (26).
(25) The host recognizes that the card is Ver2.00 or Ver3.00 Standard Capacity SD Memory Card. Optimal functions defined in Version 2.00 or higher are available. Go to Step (32).
(26) The host recognizes that the card is the High Capacity SD Memory Card or Extended Capacity Memory Card.
(27) Perform the signal voltage switch procedure and go to step (32).
(28) Check SDIO flag. If SDIO = 1, go to step (28). Otherwise, go to step (31).
(29) The host recognizes that the card is SDIO only card and go to step (30).
(30) Perform the signal voltage switch procedure and go to step (33).
(31) The host recognizes that the card is unusable.
(32) In case of memory card, CMD2 is issued to get CID and Go to Step (31).
(33) CMD3 is issued to get RCA. If the RCA number is 0, the Host should issue CMD3 again.