All interrupts that are generated by the R5FSS are
summarized in MCU_R5FSS0 Hardware Requests, along with their mapping. They
can be divided into the following groups:
- R5F CPU internal interrupts: These are described in Arm Cortex-R5 Technical Reference Manual.
- CCMR5 interrupts: These are described in Section 7.1.2.5.
- ECC аggregator interrupts: These are described in the ECC Aggregator chapter.
- RAT exception interrupt: This is described in
Section 7.1.2.7.