SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The extended Message ID (29-bit ID) filtering flow is shown in Figure 12-266. Section 12.5.1.4.10.6, Extended Message ID Filter Element describes the extended Message ID filter element.
The Remote Transmission Request (RTR) and Extended Identifier (XTD) bits of the received frames are compared against the list of configured filter elements. This is controlled by the following registers:
Note that before the filter list is executed the received identifier is ANDed with the Extended ID AND Mask (MCAN_XIDAM).
Figure 12-267 Extended Message ID Filter Path