SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The ECAP module represents one complete capture channel, which has the following independent key resources:
Multiple identical ECAP modules can be contained in a system as shown in Figure 12-280. For actual number of the ECAP modules integrated in the device, refer to ECAP Integration. The letter x within a signal or module name is used to indicate a generic ECAP instance on a device. For example, output interrupt request, ECAP1INT belongs to ECAP1, ECAP2INT belongs to ECAP2, and so forth.
Figure 12-280 Multiple ECAP Modules