SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
To support outbound proxy limits, the proxy will use internal credits for tracking resource usage. SEC_PROXY_THREAD[a]_CTL register sets the max credits each outbound proxy thread contains. When a proxy thread sends a message, the current credit count (SEC_PROXY_THREAD[a]_STATUS) decrements by 1. If the current credit count is 0, then the proxy thread is not allowed to send any more messages, and they just remain inside the proxy (so that the host can come back later when a credit has become available and quickly send the same message). When a message that was send by this proxy thread is read by an inbound proxy thread then the credit is returned to this proxy thread and the current credit count increments by 1.
For inbound proxy threads, the credits are used to track pending messages. When an outbound proxy thread sends a message that is read by this proxy thread, then the current credit count of this proxy thread is incremented by 1. A current credit count that is non zero indicates a message is pending and can be read. When the proxy thread completes the read of a message the current credit count is decremented by 1. If the current credit count is zero, then the proxy thread will read an empty message where all the data is 0s. The credit count saturates at 255, so if there can be more messages in the system for that proxy thread than 255 then multiple proxy threads should be used, or the count can become mismatched after a saturate.