SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The MII Management I/F will remain idle until enabled by setting the ENABLE bit in the CPSW3_MDIO_CONTROL_REG register. The MII Management I/F will then continuously poll the link status from within the Generic Status Register of all possible 32 PHY addresses in turn recording the results in the MDIO CPSW3_MDIO_LINK_REG register. Individual PHY’s can be enabled or disabled for polling the associated bit in the CPSW3_MDIO_POLL_EN_REG register. The CPSW3_MDIO_LINK_REG and CPSW3_MDIO_ALIVE_REG register bit values are updated on the poll of each PHY. The LINKSEL bit in the CPSW3_MDIO_USER_GROUP_USER_PHY_SEL_REG_k register determines the status input that is used. A change in the link status of the two PHYs being monitored will set the appropriate bit in the MDIO CPSW3_MDIO_LINK_INT_RAW_REG register and the MDIO CPSW3_MDIO_LINK_INT_MASKED_REG register, if enabled by the LINKINT_ENABLE bit in the CPSW3_MDIO_USER_GROUP_USER_PHY_SEL_REG_k register.
The MDIO CPSW3_MDIO_ALIVE_REG register is updated by the MII Management I/F module if the PHY acknowledged the read of the generic status register. In addition, any PHY register read transactions initiated by the host also cause the MDIO CPSW3_MDIO_ALIVE_REG register to be updated.
At any time, the host can define a transaction for the MII Management interface module to undertake using the DATA, PHYADR, REGADR, and WRITE fields in a CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k register. When the host sets the GO bit in this register, the MII Management interface module will begin the transaction without any further intervention from the host. Upon completion, the MII Management interface will clear the GO bit and set the USERINTRAW field in the CPSW3_MDIO_USER_INT_RAW_REG register corresponding to the CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k register being used. The corresponding bit in the CPSW3_MDIO_USER_INT_MASKED_REG register may also be set depending on the mask setting in the MDIO CPSW3_MDIO_USER_INT_MASK_SET_REG and CPSW3_MDIO_USER_INT_MASK_CLEAR_REG registers. A round-robin arbitration scheme is used to schedule transactions that may be queued by the host in different CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k registers. The host should check the status of the GO bit in the MDIO CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k register before initiating a new transaction to ensure that the previous transaction has completed. The host can use the ACK bit in the MDIO CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k register to determine the status of a read transaction.
It is necessary for software to use the MII Management interface module to setup the auto-negotiation parameters of each PHY attached to a MAC port, retrieve the negotiation results, and setup the CPSW3_CPSW_NU_CPSW_NU_ETH_MAC_i_PN_MAC_CONTROL_REG register in the corresponding MAC.