SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The sequence for using ADMA is shown in Figure 12-36.
Figure 12-226 Transaction Control with Data Transfer Using DAT Line Sequence (Using ADMA)(1) Create Descriptor table for ADMA in the system memory.
(2) Set the Descriptor address for ADMA in the MMCSD0_ADMA_SYS_ADDRESS register.
(3) Set the value corresponding to the executed data byte length of one block in the MMCSD0_BLOCK_SIZE register.
(4) Set the value corresponding to the executed data block count in the MMCSD0_BLOCK_COUNT register in accordance with Determination of Transfer Type.
(5) Set the argument value to the Argument register (MMCSD0_ARGUMENT1_LO and MMCSD0_ARGUMENT1_HI).
(6) Set the value to the MMCSD0_TRANSFER_MODE register. The Host Driver determines Multi/Single Block Select, Block Count Enable, Data Transfer Direction, Auto CMD12 Enable and DMA Enable in the MMCSD0_TRANSFER_MODE register. Multi/Single Block Select and Block Count Enable are determined according to Determination of Transfer Type. If response check is enabled (MMCSD0_TRANSFER_MODE[7] RESP_ERR_CHK_ENA = 1), set MMCSD0_TRANSFER_MODE[8] RESP_INTR_DIS bit to 1 and select Response Type R1/R5 (MMCSD0_TRANSFER_MODE[6] RESP_TYPE).
(7) Set the value to the MMCSD0_COMMAND register.
Note: When writing to the upper byte [3] of the MMCSD0_COMMAND register, the SD command is issued and DMA is started.
(8) If response check is enabled, go to stop (11) else wait for the Command Complete Interrupt (MMCSD0_NORMAL_INTR_STS[0] CMD_COMPLETE bit).
(9) Write 1 to the MMCSD0_NORMAL_INTR_STS[0] CMD_COMPLETE bit to clear this bit.
(10) Read Response register (MMCSD0_RESPONSE_0 - MMCSD0_RESPONSE_7) and get necessary information of the issued command.
(11) Wait for the Transfer Complete Interrupt (MMCSD0_NORMAL_INTR_STS_ENA[1] XFER_COMPLETE) and ADMA Error Interrupt (MMCSD0_ADMA_ERR_STATUS[1-0] ADMA_ERR_STATE).
(12) If MMCSD0_NORMAL_INTR_STS_ENA[1] XFER_COMPLETE bit is set to 1, go to Step (13) else if MMCSD0_ADMA_ERR_STATUS[1-0] ADMA_ERR_STATE bit field is set to 1, go to Step (14).
(13) Write 1 to the MMCSD0_NORMAL_INTR_STS_ENA[1] XFER_COMPLETE bit to clear this bit.
(14) Write 1 to the MMCSD0_ADMA_ERR_STATUS[1-0] ADMA_ERR_STATE bit field to clear this bit.
(15) Abort ADMA operation. SD card operation should be stopped by issuing abort command. If necessary, the Host Driver checks MMCSD0_ADMA_ERR_STATUS register to detect why ADMA error is generated.
Note: Step (3) and Step (4) can be executed simultaneously. Step (6) and Step (7) can also be executed simultaneously.