SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
In DMSS0_INTAGGR0, the INTAGGR will provide a set of Global event multicast (GEVI[a]_MCMAP) registers. These registers allow an ingress Global event on its ingress ETL interface to be mapped into two egress Global events on two separate egress ETL interfaces. A set of registers map the ingress Global event index (1-N) into two arbitrary egress event indices.