SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
This register selects which channel make up the input group 3. This is used for group event generation and group mode settings.
Return to Summary Table
| Instance Name | Physical Address |
|---|---|
| AASRC0 | 02D0 0080h |
| AASRC1 | 02D4 0080h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R | |||||||
| 0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R | |||||||
| 0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| CHANNEL_15_GROUP_ENABLE | CHANNEL_14_GROUP_ENABLE | CHANNEL_13_GROUP_ENABLE | CHANNEL_12_GROUP_ENABLE | CHANNEL_11_GROUP_ENABLE | CHANNEL_10_GROUP_ENABLE | CHANNEL_9_GROUP_ENABLE | CHANNEL_8_GROUP_ENABLE |
| R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
| 0h | 0h | 0h | 0h | 0h | 0h | 0h | 0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| CHANNEL_7_GROUP_ENABLE | CHANNEL_6_GROUP_ENABLE | CHANNEL_5_GROUP_ENABLE | CHANNEL_4_GROUP_ENABLE | CHANNEL_3_GROUP_ENABLE | CHANNEL_2_GROUP_ENABLE | CHANNEL_1_GROUP_ENABLE | CHANNEL_0_GROUP_ENABLE |
| R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
| 0h | 0h | 0h | 0h | 0h | 0h | 0h | 0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31:16 | RESERVED | R | 0h | Always read as 0 |
| 15 | CHANNEL_15_GROUP_ENABLE | R/W | 0h | Input Channel 15 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 14 | CHANNEL_14_GROUP_ENABLE | R/W | 0h | Input Channel 14 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 13 | CHANNEL_13_GROUP_ENABLE | R/W | 0h | Input Channel 13 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 12 | CHANNEL_12_GROUP_ENABLE | R/W | 0h | Input Channel 12 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 11 | CHANNEL_11_GROUP_ENABLE | R/W | 0h | Input Channel 11 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 10 | CHANNEL_10_GROUP_ENABLE | R/W | 0h | Input Channel 10 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 9 | CHANNEL_9_GROUP_ENABLE | R/W | 0h | Input Channel 9 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 8 | CHANNEL_8_GROUP_ENABLE | R/W | 0h | Input Channel 8 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 7 | CHANNEL_7_GROUP_ENABLE | R/W | 0h | Input Channel 7 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 6 | CHANNEL_6_GROUP_ENABLE | R/W | 0h | Input Channel 6 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 5 | CHANNEL_5_GROUP_ENABLE | R/W | 0h | Input Channel 5 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 4 | CHANNEL_4_GROUP_ENABLE | R/W | 0h | Input Channel 4 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 3 | CHANNEL_3_GROUP_ENABLE | R/W | 0h | Input Channel 3 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 2 | CHANNEL_2_GROUP_ENABLE | R/W | 0h | Input Channel 2 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 1 | CHANNEL_1_GROUP_ENABLE | R/W | 0h | Input Channel 1 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 0 | CHANNEL_0_GROUP_ENABLE | R/W | 0h | Input Channel 0 Group Enable indicates if the Input Channel is part of the group3 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Input Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |