SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The CSI_RX_IF will default to stop processing the frame whenever a header Reserved DT or ECC error is detected, or when a long packet payload CRC is identified.
The CSI_RX_IF will detect the error condition and capture the associated VC, DT and WC information for the packet header before generating an error interrupt flag on CSI_RX_IF_VBUS2APB_ERROR_IRQS.
The CSI_RX_IF will stop processing the current frame and stop the stream.