SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The PVU does not support multiple entries in a TLB that match the same virtual address. This is an illegal condition for software to program, as there is no mechanism to select one over the other. The PVU will have unpredictable results if this occurs, with the one requirement that the input transactions will never transition from a non-secure attribute to a secure attribute even in this illegal condition. This means that there is no support for background and foreground translating entries in the same TLB (which would be the result if a real MMU were used also). If software user wants to use a foreground and background method (that is not MMU compliant), he can place the foreground entries in earlier TLBs that are chained together, and the background entries are in the later TLBs, so that no single TLB has overlapping entries. The background entry would only be hit when the address falls within the background range but not any of the foreground ranges.