Perspective transforms are used to align the image data of two different cameras viewing the same scene from different positions. It can also be used in the case of stereo image rectification to align the epipolar lines of the left/right image pair with their scan lines.
The following steps need to be performed by the application to initialize and run LDC to perform perspective transform.
- Check and wait for VPAC_LDC_CTRL[2] BUSY to
become IDLE (0).
- Set VPAC_LDC_CTRL[4-3] IP_DATAMODE and
VPAC_LDC_CTRL[6-5] IP_DFMT to required data mode and format.
- If lens distortion correction is performed at the
same time as the perspective transform, set VPAC_LDC_CTRL[1] LDMAPEN = 1.
Otherwise, set LDMAPEN = 0.
- Set the input frame base address in
VPAC_LDC_RD_BASE_H / VPAC_LDC_RD_BASE_I. Note that the frame base address must
be aligned on a 16-byte boundary.
- Set the input frame line offset in
VPAC_LDC_RD_OFST[15-0] OFST.
- Set the tile size in VPAC_LDC_OUT_BLKSZ[15-8] OBH
and VPAC_LDC_OUT_BLKSZ[7-0] OBW. Note the constraints on OBW in Table 6-69.
- Set the pixel pad in VPAC_LDC_OUT_BLKSZ[19-16]
PIXPAD.
- Set the input frame size in
VPAC_LDC_INPUT_FRSZ[29-16] H and VPAC_LDC_INPUT_FRSZ[13-0] W.
- Set the output frame size in
VPAC_LDC_MESH_FRSZ[29-16] H and VPAC_LDC_MESH_FRSZ[13-0] W. Mesh data has to be
present for entire frame after transform.
- Set the output compute frame size in
VPAC_LDC_COMPUTE_FRSZ[29-16] H and VPAC_LDC_COMPUTE_FRSZ[13-0] W.
- Set the starting output point in
VPAC_LDC_INITXY[12-0] INITX and VPAC_LDC_INITXY[28-16] INITY.
- Configure SL2 Interface programming registers. Details of LSE configuration is captured in Section 6.7.4.3.4.
- If the data format is NV12, set the 420 UV input
plane base address in VPAC_LDC_RD_420C_BASE_H / VPAC_LDC_RD_420C_BASE_l. This
address must be 16-byte aligned.
- Set the mesh offset table pointer to the correct
address (VPAC_LDC_MESH_BASE_H / VPAC_LDC_MESH_BASE_l and VPAC_LDC_MESH_OFST. Set
the table down sampling factor for MxM down sampling in MESHTABLE_CFG.M.
- Set the Y plane interpolation type to bilinear or
bicubic in VPAC_LDC_CFG[6] YINT_TYP.
- Set the eight perspective transform parameters in
VPAC_LDC_AFF_AB.A, VPAC_LDC_AFF_AB.B, VPAC_LDC_AFF_CD.C, VPAC_LDC_AFF_CD.D,
VPAC_LDC_AFF_EF.E, and VPAC_LDC_AFF_EF.F. If affine transform is not used, then
these need to be set to the following values: A = 4096, B = 0, C = 0, D = 0, E =
4096, F = 0,G = 0 and H = 0. Enable VPAC_LDC_CTRL[7] PWARPEN = 1.
- Set VPAC_LDC_CTRL[0] LDC_EN = 1 to start the LDC
operation.
- Start the HTS init sequencing. LDC fetch/processing is gated with hts_init.
- Wait for VPAC_LDC_CTRL[2] BUSY to become IDLE (0)
or wait for the end of frame completion interrupt.