SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
After the first N virtIDs for DMA class usage, the remaining virtIDs up to the maximum allowed (as set in PVU_VIRTID_MAP2) are for general usage. Each of these map one to one to a TLB, where the calculation is:
There are no classes used for this range of virtIDs. An input virtID that is beyond the MAX_CNT bitfield value will produce an error.