SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
Figure 6-111 shows the architectural overview of the MSC_CORE. Each reconfigurable multi-scaling engine in the MSC_CORE receives its input frame data from its own dedicated VP (vbusp write only slave) interface. VP_IN_0 port is used for the thread #0 (multi-scaling engine-0) and VP_IN_1 port is used for the thread #1 (multi-scaling engine-1). The THREAD_MAP parameter of the MSC_LSE output channel configuration register (VPAC_MSC_LSE_DST_BUF_CFG_j[7] THREAD_MAP ) controls which input port is connected to which scaling filter (filter_0 ~ filter_9).
The scaling filter implements the vertical-before-horizontal architecture in order to avoid intermediate result line buffers that would be needed in the horizontal-before-vertical configuration. This architecture also allows the source frame width to be not restricted by internal line buffer sizes.
Each scaling filter in the MSC_CORE consists of 5-tap (32/64-phase) Polyphase filter based vertical and horizontal resizers. At the input of each resizer, a ROI checker determines the input start position (that is, marks the input data as valid). Output of each resizer is then trimmed to the configured output size of the scaling filter in each respective direction.
For MSC, the vertical input edge padding is performed in the MSC_LSE while the horizontal input boundary padding is done within the MSC_CORE before the horizontal resizer.