SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The aim of the indirect mode of operation is to read significant numbers of bytes from FLASH memory without requiring a data interface access to trigger it. Instead indirect operations are controlled and triggered by software via specific control/configuration Indirect Read Transfer registers (OSPI_INDIRECT_READ_XFER_CTRL_REG, OSPI_INDIRECT_READ_XFER_WATERMARK_REG, OSPI_INDIRECT_READ_XFER_START_REG, and OSPI_INDIRECT_READ_XFER_NUM_BYTES_REG). This block will communicate with an embedded low level SPI protocol state machine module to perform an efficient and optimized FLASH read burst, placing the read data into the local SRAM module ready for fast and low latency delivery to any external master.
By default, the Indirect Read controller is disabled. Before enabling it, software must configure how much data is required and the start address. The start address and total number of bytes to be fetched is defined in OSPI_INDIRECT_READ_XFER_START_REG and OSPI_INDIRECT_READ_XFER_NUM_BYTES_REG registers, respectively. Up to two indirect operations can be programmed at any one time. The second operation can be triggered while the first is in progress. Supporting two indirect operations allows a short turnaround time between the completion of one indirect operation and the start of the second. For more information refer to Section 12.3.2.3.10.3, Indirect Access Queuing.
The total number of bytes to read in an indirect operation is not limited by the size of the SRAM. The size of SRAM will only limit the size of requests. In the case of SRAM overrun, the controller will back pressure FLASH reads until space becomes available in the SRAM. Back pressuring the reads on the SPI interface is handled by completing any current read burst, waiting until space in the SRAM becomes available and then issuing a new read burst at the address where the previous terminated burst ended.
An external master will be able to fetch the data that the controller has read from external FLASH memory by issuing data interface reads to the OSPI module. The address of the incoming read access must be in the range of indirect trigger address programmed via the OSPI_IND_AHB_ADDR_TRIGGER_REG register to indirect trigger address + 2**(indirect trigger address range) - 1. Default value of the range is equal to 16 locations. This allows a 16-beat burst to be applied starting from the indirect trigger address. The smaller bursts are possible to handle effectively as well with this approach. Furthermore it is not strict requirement to push consecutive address sequence. Actual address just has to be in the indirect range to grant SRAM as source. Each valid Indirect Read will cause the internal SRAM to be popped, thereby decoupling the incoming read access address from the FLASH address – that is not direct mapped. Therefore the indirect trigger address does not have any relationship with the FLASH address. It is just to indicate that data should take the SRAM as source instead of the FLASH memory array after triggering of any valid Indirect Read. The FLASH address for Indirect Read is taken from the OSPI_INDIRECT_READ_XFER_START_REG register. Assuming the requested data is present in the SRAM at the point the data interface access is received by the OSPI module, then the data will be fetched from the SRAM and the response to the read burst will be achieved with minimum latency. Once the data has been read from the SRAM, the OSPI module will free up the associated resource in the SRAM.
If a read access is received whose address is not within the range described above then that access will not be completed using the indirect controller. It will instead be serviced by the direct access controller.
If a read access is received whose address is within the range described above but the requested data is not immediately present in the SRAM then wait states will be applied until the data has been read from FLASH and pushed to the SRAM.
If a read burst is received whose access elements traverse the Indirect trigger range, then the accesses within the Indirect trigger range will be processed by the indirect controller and the rest will be taken by the direct access controller. This is likely to be a software configuration error.
The external master is only permitted to issue 32-bit data interface reads until the last word of an indirect transfer. This helps keep the SRAM control logic less complex. On the final read, the external master may issue a 16-bit (Halfword) or byte access to complete the transfer. It is also permitted for the external master to always issue a 32-bit Word read on the last indirect access. The controller will pad the upper bits of the response with zero. The current expectation is that the SRAM will be kept fairly full while the read operation is carried out. The fill level of the SRAM is directly readable by software reading the OSPI_SRAM_FILL_REG register.
An indirect operation may be cancelled at any time by setting 1 to OSPI_INDIRECT_READ_XFER_CTRL_REG[1] CANCEL_FLD bit.
Any bus master should be allowed to initiate an indirect access. The OSPI module provide software access mechanism to the SRAM fill-level directly via configuration registers and then decide for itself when the data should be fetched from the local SRAM. The fill level watermark register (see OSPI_INDIRECT_READ_XFER_WATERMARK_REG register) is provided. When the SRAM fill level passes this watermark, an interrupt is generated. If the watermark value is > 0, the watermark interrupt is also generated when the final byte of data has been read by the OSPI module and placed in the SRAM, even if the actual SRAM fill level has not risen above the watermark. This last feature is useful to avoid software tracking how much data has been read and resetting the watermark value for the last few bytes of an indirect read transfer.
Two further interrupt sources are provided to help understand the status of an indirect operation. Firstly, an interrupt is generated when an indirect operation has completed. Secondly, an interrupt is generated if an Indirect Read operation was requested but could not be accepted due to the fact 2 indirect operations have already been buffered by the OSPI module.
Setting the OSPI_INDIRECT_READ_XFER_CTRL_REG[0] START_FLD bit starts an indirect read operation. OSPI_INDIRECT_READ_XFER_CTRL_REG[2] RD_STATUS_FLD bit is available to check the status.