SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The interconnect supports capturing null slave errors for reporting. A null slave error occurs when a transaction does not address any slaves based on the address map, resulting in the transaction returning error status. The null errors are captured into registers and an interrupt is generated. There is only one set of reporting registers, so only one error can be captured until cleared by software. The report captures some details of the transaction, such as the Route ID to identify the master involved and the address accessed. See Null Error Reporting Registers for details about the null error reporting registers.