SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
DSS7 is capable of driving multiple displays in parallel through a combination of interfaces:
The following diagram shows how the 4 video outputs (P[4:1]) of the DSS are mapped to the various display peripherals on the device. The DSS internal registers determine which of the display peripherals are allowed to output content at any time so that content protection is supported through the DSS built-in security capabilities.