SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The first step of the module is to map the transaction to a specific TLB by comparing the virtID, chanID upper bits, and those programmed in PVU_VIRTID_MAP1 and PVU_VIRTID_MAP2. This mapping determines which TLB to select from the virtID. That TLB is used for the remainder of the pipeline. If there is no match then the PVU automatically misses.