SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The stimulus port on the STM supports 64 independent master interfaces that are each 24-bits wide:
In order to minimize the address footprint of the STM and also to ease SW development, the source of the transaction request is used to select the master space. As such, the upper bits of the STM stimulus port [29:24] are derived from the bus ID of the message source.