SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
An unsupported feature error is returned for a TR that is received that cannot be run because it specifies a feature that is optional and not supported by the UTC that received the TR. The STATUS FIELD specifies the feature that was not supported. If it specifies multiple features that were not supported the UTC implementation can determine which type it wants to return
Value | Submission Error Type |
---|---|
0 | TR Type not supported |
1 | STATIC not supported |
2 | EOL not supported |
3 | CONFIGURATION SPECIFIC not supported |
4 | AMODE not supported |
5 | ELTYPE not supported |
6 | DFMT not supported |
7 | SECTR not supported |
8 | AMODE SPECIFIC Field not supported |
9-15 | Reserved |