SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The EQEP peripheral includes an integrated edge capture unit to measure the elapsed time between the unit position events as shown in Figure 12-304. This feature is typically used for low speed measurement using the following equation:
where,
The EQEP capture timer (QCTMR bitfield in EQEP_QCTMR register) runs from prescaled SYSCLKOUT and the prescaler is programmed by the EQEP_QCAP_QPOS_CTL[6-4] CCPS bits. The capture timer QCTMR value is latched into the capture period register (EQEP_QC_PRD_TLAT) on every unit position event and then the capture timer is reset.
Time measurement (ΔT) between unit position events will be correct if the following conditions are met:
The capture unit sets the EQEP overflow error flag (EQEP_QEP_STS_CT[3] COEF) in the event of capture timer overflow between unit position events. If a direction change occurs between the unit position events, then an error flag is set in the status register (EQEP_QEP_STS_CT[2] CDEF).
Capture Timer (EQEP_QCTMR register) and Capture period register (EQEP_QC_PRD_TLAT) can be configured to latch on following events.
If the EQEP_QDEC_QEP_CTL[18] QCLM bit is cleared, then the capture timer and capture period values are latched into the EQEP_QC_PRD_TLAT and EQEP_QCPRDLAT registers, respectively, when the CPU reads the position counter in EQEP_QPOSCNT.
Capture timer and capture period values are not latched for an emulation read.
If the EQEP_QDEC_QEP_CTL[18] QCLM bit is set, then the position counter, capture timer, and capture period values are latched into the EQEP_QPOSLAT, EQEP_QC_PRD_TLAT and EQEP_QCPRDLAT registers, respectively, on unit time out.
Figure 12-306 shows the capture unit operation along with the position counter.
The EQEP_QCAP_QPOS_CTL register should not be modified dynamically (such as switching CAPCLK prescaling mode from SYSCLKOUT/4 to SYSCLKOUT/8, where SYSCLKOUT is equivalent to EQEPx__FICLK). The capture unit must be disabled before changing the prescaler.
Velocity Calculation Equations:
where
v(k): Velocity at time instant k
x(k): Position at time instant k
x(k-1): Position at time instant k - 1
T: Fixed unit time or inverse of velocity calculation rate
ΔX: Incremental position movement in unit time
X: Fixed unit position
ΔT: Incremental time elapsed for unit position movement
t(k): Time instant "k"
t(k-1): Time instant "k - 1"
Unit time (T) and unit period (X) are configured using the EQEP_QUPRD and EQEP_QCAP_QPOS_CTL[3-0] UPPS registers. Incremental position output and incremental time output is available in the EQEP_QPOSLAT and EQEP_QCPRDLAT registers.
Parameter | Relevant Register to Configure or Read the Information |
---|---|
T | Unit Period Register (EQEP_QUPRD) |
ΔX | Incremental Position = QPOSLAT(k) - QPOSLAT(k - 1) |
X | Fixed unit position defined by sensor resolution and QCAPCTL[3-0] UPPS bits |
ΔT | Capture Period Latch (QCPRDLAT) |