SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
A channel must be torn down through setting the DRU_CHRT_CTL_j[30] TEARDOWN bit to 0x1. This allows for channel reconfiguration. Setting the TEARDOWN bit to 0x1 forces the channel to stop sending any new requests not already in the pipeline and when all outstanding requests have been received all other bits in the DRU_CHRT_CTL_j register are cleared. If the DRU_CFG_j[31] PAUSE_ON_ERR bit is set and an error occurs the tear down mechanism can be used to restart the channel. The TEARDOWN bit being set to 0x1 also makes the TR STATIC field in any future reads from the TR memory to be set to 0x0 no matter the value when the TR was submitted. This is the mechanism used to stop a static TR.