SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The DPHY_TX may have the capability to swap the data pin polarity or invert the clock lane polarity - the CSI_TX_IF_DPHY_CFG1 register is available within the controller for driving these pad level controls (using the DPHY_DIFF_INVERT_* fields). The DPHY_TX will identify any contention issues with the transmitter and flag this using the contention signals and error interrupt - this may be used by software to determine if the data pin or clock lane polarity switching is required or not (by optimizing to the minimum, preferably zero, rate of occurrence of contention issues).
Int the DPHY_TX, the IO pads for the clock and data lanes support swapping of the polarity of the signals DP-DN. All dphy_differential_invert_* outputs should be treated as asynchronous. Note that, if these signals need to be asserted, they should be asserted before releasing the DPHY_TX reset.
Each lane can be controlled independently with the CSI_TX_IF_DPHY_CFG and CSI_TX_IF_DPHY_CFG1 registers.