SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
If a target read for a message returns a bus error, this indicates the read was bad and the data is corrupt and usually 0s. Because the private word in contained in the message, if the private word is corrupted then the source proxy thread is not valid and the credit return will not be correct. Since the data is usually 0, this means the credit would be returned to proxy thread 0 incorrectly most of the time. And the credit will be lost for the actual source proxy thread of the message that was not read correctly. The hardware has no way to correct for this, as the message from the target is corrupt so it does not know the correct owner of the credit. If software detects that a read message is corrupt, it can attempt to correct the situation by resetting the affected proxy threads using that queue, to restore their credit counts back to the default. Software may also want to reset proxy thread 0 since it may be getting extra credits.