There are three priorities that are used inside the Gigabit Ethernet Switch: packet priority, header packet priority, and switch priority. The header packet priority is used as the outgoing VLAN priority if the packet is egressing from the switch with a VLAN tag. The switch priority determines which of the 8 FIFO priority queues the packet uses during egress.
Figure 12-64 below, as well as the corresponding explanation that follows, explains each of the priorities, how they are determined, and how they are used. A number in parentheses in the figure indicates a process (Ethernet port ingress, host port egress, etc.). Each bullet in the text following the diagram explains one of the 5 processes pointed out in the figure.
From Figure 12-64 above:
- (1) is the ingress process that occurs at the external Ethernet ports
- The incoming packet is assigned a packet
priority based on either its VLAN priority, IPv4 or IPv6 DSCP
value, or the ingress port’s priority. This packet priority is
then mapped to a header packet priority using the
CPSW_PN_RX_PRI_MAP_REG register where N is the port where the packet
entered the switch. This process is explained in further detail in Section 12.2.1.2.6.2.
- (2) is the egress process that occurs at the external Ethernet ports
- If the switch is in VLAN Aware mode then the VLAN header may be added, replaced, or removed during the egress process. If the VLAN header is to be added or replaced, the VLAN priority will come from the header packet priority that was determined in process (1) or (5). Transmit VLAN processing is the same for both the host port and the external Ethernet ports and is described in Section 12.2.1.2.6.4.1.
- (3) is the process by which it is decided which priority TX queue to place the packet on in the Port N TX FIFO during egress
- Each Port’s TX FIFO has 8 queues that each
correspond to a priority that is used when determining which packet will
egress from the switch next at that port. The header packet
priority (Ethernet port ingress, process (1)) or the receive
packet thread (host port 0 ingress, process (5)) gets mapped through the
CPSW_PN_RX_PRI_MAP_REG register (where N is the egress port number) to
determine the switch priority of the packet. The switch
priority determines which TX FIFO queue to place the packet in.
The FIFO architecture is described in Section 12.2.1.2.6.10.11. The header packet priority to switch priority mapping is discussed
in Section 12.2.1.2.6.2.
- (4) is the egress process that occurs at Host Port 0 toward the transmit streaming interface (TXST)
- The TXST has 8 egress threads for each external Ethernet port (32 threads in a 5-port switch and 64 threads in a 9-port switch). The TX thread that is selected for a packet is determined by the Ethernet port of ingress and the switch priority of the packet that was determined in process (3).
- If the switch is in VLAN Aware mode then the VLAN header may be added, replaced, or removed during the egress process. If the VLAN header is to be added or replaced, the VLAN priority will come from the header packet priority that was determined in process (1). Transmit VLAN processing is the same for both the host port and the external Ethernet ports and is described in Section 12.2.1.2.6.4.1.
- (5) is the ingress process that occurs at Host Port 0
- The incoming packet is assigned a packet
priority based on either its VLAN priority, IPv4 or IPv6 DSCP
value, or the host port’s priority. This packet priority is then mapped
to a header packet priority using the CPSW_PN_RX_PRI_MAP_REG
register.
- Host port 0 also has a received packet thread. The receive packet thread is based on either the packet’s VLAN priority, IPv4 or IPv6 DSCP value, or the streaming interface (RXST) thread that the packet entered host port 0 on.