SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
In UYVY and NV12 mode, the pixel interpolation type can be set to bi-cubic interpolation for best quality or bilinear interpolation for faster performance.
As the coordinates ( hd,vd) calculated by the back-mapping function are not generally integer values, bi-cubic or bilinear interpolation is applied to the distorted pixels.
Depending on register configuration, bi-cubic or bilinear interpolation is used to interpolate the output Y pixels:
In the case of bi-cubic interpolation, the distorted pixel is interpolated from the 16 Y pixels in the 4 x 4 grid around the distorted location, as shown in Figure 6-87. Bi-cubic interpolation is used first along the horizontal direction, then the vertical direction.
If bi-linear interpolation is selected, the distorted pixel is interpolated from the four Y pixels in the 2 x 2 grid around the distorted location, as shown in Figure 6-88.
For Cb and Cr components, simple bilinear interpolation is used. Each distorted pixel is interpolated from the four same-color pixels on the 2 x 2 grid around the distorted location. For UYVY data, the Cb/Cr grid is not square, but is 2x wider compared to the height. This is shown in Figure 6-89.