SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The CSI_RX_IF will use the monitor control (CSI_RX_IF_VBUS2APB_STREAM0_MONITOR_CTRL - CSI_RX_IF_VBUS2APB_STREAM3_MONITOR_CTRL) or STOP mechanism to stop the stream processing at the end of the active frame. The stream monitor, configuration and interrupt registers can be redefined and then the stream restarted. The pixel interface will begin processing at the next frame start.
The FW will use the FCC config control register (CSI_RX_IF_VBUS2APB_STREAM0_FCC_CFG - CSI_RX_IF_VBUS2APB_STREAM3_FCC_CFG) to perform a start and stop as soon as a frame count is detected. The FCC config control register will define the start and stop frame count and the stream will identify when these values are matched. The stream output will begin when start frame is detected and then stop once the stop frame is reached. The virtual channel can be defined in CSI_RX_IF_VBUS2APB_STREAM0_FCC_CTRL - CSI_RX_IF_VBUS2APB_STREAM3_FCC_CTRL[4-1] FCC_VC, and must match the virtual channels that are available to the stream in the CSI_RX_IF_VBUS2APB_STREAM0_DATA_CFG - CSI_RX_IF_VBUS2APB_STREAM3_DATA_CFG register.
The frame capture is enabled when CSI_RX_IF_VBUS2APB_STREAM0_FCC_CTRL - CSI_RX_IF_VBUS2APB_STREAM3_FCC_CTRL[0] FCC_EN is set ‘1’
The FW can check the current frame counter value from the CSI_RX_IF_VBUS2APB_STREAM0_FCC_CTRL - CSI_RX_IF_VBUS2APB_STREAM3_FCC_CTRL[31:16] FRAME_COUNTER