SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
When operating as a PCIe End Point, the device will be located in PCIe memory map at location programmed in the Base Address Registers by the PCIe Root device. Any PCIe transactions destined for the device from the upstream ports will get transferred to the master port on the PCIe subsystem. Similarly, any transactions originating from the software will be sent over to PCIe link.
In End Point mode, the PCIe subsystem provides address translation functionality. It is possible to map memory accesses originating on PCIe side to memory accesses with different address on the CBA bus side. These address ranges are configurable through application registers.