SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The Host is ultimately responsible for providing all of the free descriptors and buffers that the port uses as it receives packets. For Rx Free Descriptor/Buffer queues, descriptors are allocated in a large block by the Host and then initialized and linked with buffers before being given matched pairs where the Host initializes the descriptor to point to its corresponding buffer before being pushed onto a Receive Free Descriptor/Buffer queue. Once the host has allocated both a descriptor and a buffer, it adds them to an Rx Free Descriptor/Buffer Queue by writing the pointer to the descriptor to the Rx Free Descriptor/Buffer Queue register D for the desired queue.
Before the Host adds each Rx buffer descriptor to the queue, it must first initialize the Rx buffer descriptor values as follows:
Depending on the software architecture, the Host may also desire to write the return policy bit in the descriptor at this point as well. The DMA will not overwrite any of these listed fields (including return policy) during reception.
All other fields in the Descriptor do not need to be initialized as they will be overwritten by the Port on reception.