SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The read enable (REN) input to the RAMs instantiated in this module are constantly tied to 1’b1. As a result, read is continuously in progress.
In order to test ECC single error injection on a particular RAM row, the following conditions have to be maintained before setting the ADC_ECC_CTRL[3] FORCE_SEC bit: