SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
Similarly, the receive data ready flag - RDATA in the MCASP_RSTAT register reflects the data ready status of XRBUFn buffers for all of the active slot receiving serializers. The RDATA flag is set whenever data is transferred from a receiving serializer shift register XRSRn to its corresponding XRBUFn data buffer. Thus, the RDATA bit indicates the global event that some of the receivers data buffer - RXBUFn already contains received data (this is, a buffer is full) and is ready to transfer it to the host. The receive data ready event is individually indicated per serializer in its corresponding control register MCASP_SRCTLn [5] RRDY status bit. When this bit is set to 0b1, it notifies to host that this serializer Rx buffer must be serviced (read). When MCASP_RBUFn register is read from the host, the MCASP_SRCTLn [5] RRDY bit is deasserted to 0b0. As RDATA global flag is an OR-event of all active serializers RRDY flags, it indicates to software the moment, when read service operation has to be initiated by the MCASP host (RDATA = 0b1). The RRDY flags have to be sequentially scanned by user software to determine which serializer MCASP_RBUFn register has to be currently read. Once all requested MCASP_RBUFn registers are read, the serializers control RRDY flags are cleared to 0b0. As a consequence, RDATA flag is deasserted to 0b0, to indicate to SW that read operation is completed for all serializers.
The global RDATA flag can be cleared when the MCASP_RSTAT[5] RDATA bit is written to 0b1, or once MCASP_RBUFn registers of all the serializers, that have previously raised their RRDY flags, are read by the host.
Whenever RDATA flag is set, the RINT event is automatically generated on MCASP[0-2]_REC_DMA_EVT line (if enabled in the MCASP_PIDTCTL register) to notify the DMA of the MCASP_RBUFn full status. An interrupt - MCASP[0-2]_REC_INTR_PEND can be also generated if the RDATA interrupt is enabled in the MCASP_RINTCTL register (for details, see Section 12.5.2.3.13.1, Receive Data Ready Interrupt).
Figure 12-339 shows the timing details of when RINT event is generated at the MCASP boundary. In this example, as soon as the last bit (bit A0) of Word A is received, the MCASP sets the RDATA flag and generates an RINT event. However, it takes up to five MCASP interface clocks (RINT Latency) before RINT is active at the MCASP boundary. Upon RINT, the CPU can begin servicing the MCASP by reading Word A from the MCASP_RBUFn (service time). The CPU must read Word A from the MCASP_RBUFn register no later than the setup time required by the MCASP (Setup Time) (n = 0 to 15).
The maximum service time (see Figure 12-339) can be calculated as:
Service Time = Time Slot - RINT Latency - Setup Time