Figure 6-123 shows the core of the Noise filter. The line buffers are stored in SL2.
There are two modes of filtering:
- Bilateral filtering mode: The overall weights are computed based on center pixels. These are 8-bit unsigned weights. The center weight is read from MMR as 8-bit unsigned. The 9th bit for all weight is hardwired to '0'. The MAC operation is signed multiply with addition. As MSB for weight is set '0', it will be act as unsigned multiplier of 12-bit pixel to 8-bit unsigned weight.
- Generic filtering mode: In this mode, all weights are 9-bit signed value read LUT from initial 24 values read as 9-bit signed value from every 2 bytes (16 bits) locations.