SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
After reset, all threads on PSI-L are uninitialized and unpaired. The host will pair each source PDMA channel with (typically) a corresponding destination channel in the paired-DMA. The PDMA thread is configured to point to the paired-DMA thread and the paired-DMA thread is configured to point to the PDMA thread. Once paired, the source channels in the PDMA will send all their data to the source channel in the paired-DMA and the destination channel in the paired-DMA will never see any data other than data from the source channel in the PDMA.
Refer to their descriptions for further details.