The EST can be configured to generate CPTS
timestamp events for selected express traffic. The EST timestamp events use the CPTS
host event type (CPSW_CPTS_EVENT_1_REG[23-20] EVENT_TYPE = 7 decimal. The EST
timestamps will not override host sent timestamps for packets that were sent from
the host with an enabled host timestamp.
- EST Events (host events) contain the below information:
- Time Stamp of the selected express packet.
- The event CPSW_CPTS_EVENT_1_REG[28-24]
PORT_NUMBER indicates the transmit port number.
- The event CPSW_CPTS_EVENT_1_REG[23-20] EVENT_TYPE
is decimal 7 (host event).
- The event CPSW_CPTS_EVENT_1_REG[23-20]
MESSAGE_TYPE indicates the packet transmit hardware switch
priority.
- The event CPSW_CPTS_EVENT_1_REG[15-0] SEQUENCE_ID
upper nibble indicates the packet receive port number.
- The event CPSW_CPTS_EVENT_1_REG[15-0] SEQUENCE_ID
lower byte indicates the sequence number of the express packet in
numerical order. The first event is event one, the second is event
two and so on. The sequence ID rolls over to zero after 0xFF
(8-bits).
- The event domain is the value from the
CPSW_EST_TS_DOMAIN_REG[7-0] EST_TS_DOMAIN register.
- When CPSW_PN_EST_CONTROL_REG_k[2] EST_TS_EN is
set, timestamp events will be generated on selected express traffic.
- When CPSW_PN_EST_CONTROL_REG_k[3] EST_TS_FIRST is
also set, events will be generated only on the first express packet in each
time interval. If CPSW_PN_EST_CONTROL_REG_k[4] EST_TS_ONEPRI is also set
then the event will only be on the first CPSW_PN_EST_CONTROL_REG_k[7-5]
EST_TS_PRI express packet in the time interval. If
CPSW_PN_EST_CONTROL_REG_k[4] EST_TS_ONEPRI is clear then the event will be
generated on the first express packet in the time interval on any
priority.
- When CPSW_PN_EST_CONTROL_REG_k[3] EST_TS_FIRST is
clear, events will be generated on every express packet. If
CPSW_PN_EST_CONTROL_REG_k[4] EST_TS_ONEPRI is set then the event will be
generated on every CPSW_PN_EST_CONTROL_REG_k[7-5] EST_TS_PRI express packet.
If CPSW_PN_EST_CONTROL_REG_k[4] EST_TS_ONEPRI is clear then event will be
generated on every express packet on any priority.