SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The following interrupts are generated by the NF module (see Table 6-86):
Interrupt | Description |
---|---|
NF_FRAME_DONE | Frame processing complete. |
NF_SL2_READ_ERROR | Set whenever there is an error response on VBUSM read command request for any input channel. |
NF_SL2_WRITE_ERROR | Set whenever there is an error response on VBUSM write command request for any output channel. |
All interrupts are single pulse event signals that are mapped to the VPAC level interrupt aggregation logic.