SPRUJ83D December 2023 – January 2026 AM62P , AM62P-Q1
This register describes the FIFO list to be processed for this TX channel.
| Bits | Field | Reset | Description |
|---|---|---|---|
| 31 | GroupMode | 0x0 | When set, the channel is in 'Group Mode'. It will look for Group Mode DMA requests, and access the Group Mode FIFOs. When clear, the channel is 'Stream Mode'. It will look for Stream FIFO DMA requests, and access the Stream Mode FIFOs. |
| 30 | DmaReqReset | 0x0 | When set, resets any latched DMA request using the DmaReqMask. This bit is self-clearing. It should be used to synchronize the AASRC event status with the PDMA in the event that the AASRC has been previously used and it is not known if the PDMA may have latched, and is holding, previous DMA requests. |
| 23:20 | LastSlot | 0x0 | This is the index (0-15) of the last slot in the TX FIFO ordering table used by this channel. The ordering table is read to get the FIFO index to access for each slot, starting with the first and ending with the last. |
| 19:16 | FirstSlot | 0x0 | This is the index (0-15) of the first slot in the TX FIFO ordering table used by this channel. The ordering table is read to get the FIFO index to access for each slot, starting with the first and ending with the last. |
| 15:0 | DmaReqMask | 0x0 | This field holds a set of flags indicating which AASRC DMA requests must fire in order for this channel to activate. In Steam Mode, these 16 flags correspond to the 16 DMA requests for each TX FIFO. The flags corresponding to all TX FIFOs involved with the channel should be set to 1. In Group Mode, these flags indicate which Group Mode DMA requests must fire. In this case, only bits 3:0 are relevant and only one bit should be set to 1 as a DMA channel only services a single group. |