SPRUJ83D December 2023 – January 2026 AM62P , AM62P-Q1
This is the offset of the destination address from the initial destination address for the first access of the second loop. This will be added to the destination address from the loop before. This is a signed value so that the destination address can be both above and below the initial destination address.