SPRUJ83D December 2023 – January 2026 AM62P , AM62P-Q1
The device supports HFOSC0 clock loss circuitry to detect when HFOSC0_CLK stops toggling. Dedicated hardware logic monitors HFOSC0 clock using CLK_12M_RC clock. When HFOSC0_CLK stops toggling for 9 CLK_12M_RC clock periods, a HFOSC0 clock stop loss condition is detected. If CTRLMMR_MCU_PLL_CLKSEL[8] CLKLOSS_SWTCH_EN is set , the reference clock is switched from HFOSC0_CLKOUT to CLK_12M_RC to allow the device to operate with a slower clock. The HFOSC0_CLK clock loss condition is reported as an error to MCU_ESM0 regardless of the value of MCU_CTRL_MMR_CFG0_MCU_PLL_CLKSEL[8] CLKLOSS_SWTCH_EN. Integration diagram of HFOSC0 clock loss detection is presented in Figure 6-40.
MCU_ESM0 can optionally generate an interrupt to MCU_R5FSS and DM_R5FSS0 so they can save some critical contents such as error logging to scratch pad memory or external flash. ESM must also be configured to report this error on the MCU_ERRORn pin.
HFOSC0 clock loss is a catastrophic failure since this clock is the most critical system clock. During the clock loss condition an external system intervention is required.
The clock loss mux is not a glitch free mux. The mux control is synchronized to the CLK_12M_RC clock. Since HFOSC0_CLK has stopped switching the mux should transition to RC Clock without producing glitches.
During clock-loss condition, the device reports the error to the external device through MCU_ERRORn pin - the pin is driven Low. The recovery mechanism is up to the external system (such as a PMIC to take action). For example, it can try a full system power cycle to see if the system recovers. If the system does not recover then, it has to take some other action such as to check system clocks, external crystal or supply rails.
Device PLLs will lose lock when clock loss is detected. During this time 12.5-MHz RC clock is output through the bypass muxes. The PLL will relock to a new frequency based on 12.5 MHz RC clock.
In an event of clock glitch which may potentially hang the device, then the SMS watchdog timer will expire and will generate an internal reset for the whole device.