SPRUJ83D December 2023 – January 2026 AM62P , AM62P-Q1
The Host initiates a RX channel teardown by setting the tdown bit in the RT enable register for the target RX channel. The PDMA communicates the teardown state to the UDMA-P through the PSI-L data channel, to ensure that the teardown is not seen by the UDMA-P until all the previous PDMA data for the channel has been flushed.
The PDMA does not stop reading peripheral data until it reaches a FIFO boundary, as configured through the 'X' and 'Y' parameters in the static TR. It always attempts to complete the 'Y' count for the current event being processed. Upon reaching a stopping point, the PDMA then clears the enable bit in the pairing register; however, the teardown bit remains set. No further packet processing occurs until the Host re-configures the channel. The teardown process propagates to the UDMA-P and its final status can be checked there.