SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
The next step of the module is to check the input address, which uses the bits just above the 4-kB size, bits 12 and up, as the virtual address base. This is compared against all the TLB entries for that TLB, given the size in each entry. The size affects which address bits need comparing for an entry. The minimum size of 4 kB, so address bits 12 and up are compared. But if the size is 64 kB, then bits 16 and up are compared, as the lower bits fall into the size of the page. In addition to the address, the psecure bit is used to match against the secure level of the transaction. Only secure transaction are allowed to match an entry with psecure set, while only non-secure transactions are allowed to match an entry with psecure clear. If the entry is valid and the base compare matches and the secure level matches then the entry is used for the translation and checks.