SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
Table 11-88 lists the memory-mapped registers for the TIMERMGR_CFG_CFG. All register offset addresses not listed in Table 11-88 should be considered as reserved locations and the register contents should not be modified.
CFG MMR definitions
Instance | Base Address |
---|---|
NAVSS0_TIMERMGR0_CFG | 30E8 0000h |
NAVSS0_TIMERMGR1_CFG | 30E8 1000h |
Offset | Acronym | Register Name | NAVSS0_TIMERMGR0_CFG Physical Address | NAVSS0_TIMERMGR1_CFG Physical Address |
---|---|---|---|---|
0h | TIMERMGR_PID | Peripheral ID register | 30E8 0000h | 30E8 1000h |
4h | TIMERMGR_CNTL | Timer manager control | 30E8 0004h | 30E8 1004h |
8h | TIMERMGR_COUNTER | The current counter value | 30E8 0008h | 30E8 1008h |
A0h | TIMERMGR_TIMEOUT_STATUS0 | Must be read whenever the timer interrupt fires | 30E8 00A0h | 30E8 10A0h |
A4h | TIMERMGR_TIMEOUT_STATUS1 | Contains the IDs of the second and third timers to expire | 30E8 00A4h | 30E8 10A4h |
A8h | TIMERMGR_TIMEOUT_STATUS_BANK0 | Contains the status of each timer bank for banks 31-0 | 30E8 00A8h | 30E8 10A8h |
100h + formula | TIMERMGR_STATUS_y | Each bit is the timeout status for an individual timer | 30E8 0100h + formula | 30E8 1100h + formula |
TIMERMGR_PID is shown in Figure 11-46 and described in Table 11-90.
Return to Summary Table.
This is the standard TI peripheral ID register that exists at address 0 in the peripheral space
Reset = 66F8 B100h
Instance | Physical Address |
---|---|
NAVSS0_TIMERMGR0_CFG | 30E8 0000h |
NAVSS0_TIMERMGR1_CFG | 30E8 1000h |
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
SCHEME | BU | FUNCTION | |||||||||||||
R-1h | R-2h | R-6F8h | |||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RTL_VER | MAJOR_REV | CUSTOM | MINOR_REV | ||||||||||||
R-16h | R-1h | R-0h | R-0h | ||||||||||||
LEGEND: R = Read Only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-30 | SCHEME | R | 1h | scheme |
29-28 | BU | R | 2h | bu identifier |
27-16 | FUNCTION | R | 6F8h | function identifier |
15-11 | RTL_VER | R | 16h | RTL version number |
10-8 | MAJOR_REV | R | 1h | Major revision number |
7-6 | CUSTOM | R | 0h | custom |
5-0 | MINOR_REV | R | 0h | Minor revision number |
TIMERMGR_CNTL is shown in Figure 11-47 and described in Table 11-92.
Return to Summary Table.
This register controls the overall behavior of the timer manager module
Instance | Physical Address |
---|---|
NAVSS0_TIMERMGR0_CFG | 30E8 0004h |
NAVSS0_TIMERMGR1_CFG | 30E8 1004h |
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R/W-X | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R/W-X | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | MASS_ENABLE | RESERVED | MAX_TIMER | ||||
R/W-X | W-0h | R/W-X | R/W-3FFh | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
MAX_TIMER | ENABLE | ||||||
R/W-3FFh | R/W-0h | ||||||
LEGEND: R/W = Read/Write; W = Write Only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-13 | RESERVED | R/W | X | |
12 | MASS_ENABLE | W | 0h | Always reads zero. When a 1 is written to this bit, all timers from 0 to the MAX_TIMER will be enabled. Useful for initial programming, to not need to loop over every TIMERMGR_CONTROL_j_k register to enable every timer if many or all are being used. This should only be used during initialization, or when ENABLE is set to 0, as this does not set the timers, only enable them |
11 | RESERVED | R/W | X | |
10-1 | MAX_TIMER | R/W | 3FFh | The maximum timer that will be checked - e.g. if only using 512 timers, set this to 511. All timers above this number will be ignored. Should be set once during initialization |
0 | ENABLE | R/W | 0h | Enables the timer manager. When this bit is zero, the timers will all be halted and will not count 0h = Timer Manager is disabled 1h = Timer Manager is enabled |
TIMERMGR_COUNTER is shown in Figure 11-48 and described in Table 11-94.
Return to Summary Table.
This register contains the current TIMERMGR_COUNTER value
Instance | Physical Address |
---|---|
NAVSS0_TIMERMGR0_CFG | 30E8 0008h |
NAVSS0_TIMERMGR1_CFG | 30E8 1008h |
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
VAL | |||||||||||||||||||||||||||||||
R-0h | |||||||||||||||||||||||||||||||
LEGEND: R = Read Only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | VAL | R | 0h | The current timer_counter value, in the timebase being used by all timers in this module |
TIMERMGR_TIMEOUT_STATUS0 is shown in Figure 11-49 and described in Table 11-96.
Return to Summary Table.
This register should be read whenever the timer interrupt fires. It indicates the total number of timers that have expired and the ID of the first timer to expire. If NUM_EXPIRED_TIMERS is 1, this is the only register that needs to be read. Depending on the value of NUM_EXPIRED_TIMERS, either TIMERMGR_TIMEOUT_STATUS1 or TIMERMGR_TIMEOUT_STATUS_BANK0 may be read by the software to avoid needing to read all 32 TIMERMGR_STATUS_y registers.
Instance | Physical Address |
---|---|
NAVSS0_TIMERMGR0_CFG | 30E8 00A0h |
NAVSS0_TIMERMGR1_CFG | 30E8 10A0h |
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-X | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
VALID0 | EXPIRED_TIMER0 | ||||||
R-0h | R-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
EXPIRED_TIMER0 | NUM_EXPIRED_TIMERS | ||||||
R-0h | R-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
NUM_EXPIRED_TIMERS | |||||||
R-0h | |||||||
LEGEND: R = Read Only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-24 | RESERVED | R | X | |
23 | VALID0 | R | 0h | 1 indicates that expired_timer0 is a valid expired timer. If num_expired_timers > 0, this should always be a 1 |
22-12 | EXPIRED_TIMER0 | R | 0h | The ID of the first timer to expire |
11-0 | NUM_EXPIRED_TIMERS | R | 0h | The total number of expired timers |
TIMERMGR_TIMEOUT_STATUS1 is shown in Figure 11-50 and described in Table 11-98.
Return to Summary Table.
This register contains the IDs of the second and third timers to expire. It is indended as a more efficient way of finding the first few timers to expire rather than needing to read the status of all 1024 timers.
Instance | Physical Address |
---|---|
NAVSS0_TIMERMGR0_CFG | 30E8 00A4h |
NAVSS0_TIMERMGR1_CFG | 30E8 10A4h |
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-X | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
VALID2 | EXPIRED_TIMER2 | ||||||
R-0h | R-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
EXPIRED_TIMER2 | VALID1 | EXPIRED_TIMER1 | |||||
R-0h | R-0h | R-0h | |||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
EXPIRED_TIMER1 | |||||||
R-0h | |||||||
LEGEND: R = Read Only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-24 | RESERVED | R | X | |
23 | VALID2 | R | 0h | 1 indicates that expired_timer2 is valid |
22-12 | EXPIRED_TIMER2 | R | 0h | The ID of the third timer to expire |
11 | VALID1 | R | 0h | 1 indicates that expired_timer1 is valid |
10-0 | EXPIRED_TIMER1 | R | 0h | The ID of the second timer to expire |
TIMERMGR_TIMEOUT_STATUS_BANK0 is shown in Figure 11-51 and described in Table 11-100.
Return to Summary Table.
This register contains the status of each timer bank for banks 31:0. When servicing the timer interrupt, if the num_expired_timers bit is greater than 3, this register may be read to see which banks contain expired timers. The TIMERMGR_STATUS_y registers corresponding to those banks may then be read.
Instance | Physical Address |
---|---|
NAVSS0_TIMERMGR0_CFG | 30E8 00A8h |
NAVSS0_TIMERMGR1_CFG | 30E8 10A8h |
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
VAL | |||||||||||||||||||||||||||||||
R-0h | |||||||||||||||||||||||||||||||
LEGEND: R = Read Only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | VAL | R | 0h | A 1 in bit N indicates that the corresponding bank has expired timers |
TIMERMGR_STATUS_y is shown in Figure 11-52 and described in Table 11-102.
Return to Summary Table.
Each bit is the timeout status for an individual timer. 0 = timer has not timed out or is disabled, 1 = timer has timed out
Offset = 100h + (y * 4h); where y = 0h to 1Fh
Instance | Physical Address |
---|---|
NAVSS0_TIMERMGR0_CFG | 30E8 0100h + formula |
NAVSS0_TIMERMGR1_CFG | 30E8 1100h + formula |
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
VAL | |||||||||||||||||||||||||||||||
R-0h | |||||||||||||||||||||||||||||||
LEGEND: R = Read Only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | VAL | R | 0h | Each bit is the timeout status for an individual timer |