SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
All ports
The total number of frames received on a port that were dropped by the ALE (the ALE did not forward the packet to any port). Port mask drop frame is defined to be:
This statistic does not count in the overall total as it includes every packet received greater than 32 bytes that had a zero PORT_MASK.