SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
Each interrupt has a priority number assigned to it (set using the R5FSS_VIM_PRI_INT_j register). Legal values are 0 to 15, where 0 is the highest priority and 15 is the lowest priority. The highest priority interrupt is the pending interrupt with the smallest priority number. If two pending interrupts have the same priority, the interrupt lowest numerically (0 through maximum number of interrupts) is prioritized. IRQs and FIQs are prioritized separately.
The VIM supports the interruption of the currently active interrupt by one with a higher priority. FIQs and IRQs are completely separate but both use the same mechanism.
When an interrupt goes from pending to active (FIQ: reading the R5FSS_VIM_FIQVEC register; IRQ: reading the R5FSS_VIM_IRQVEC register, or the coreN_IRQACK going high), then the interrupt is loaded into the corresponding active register (R5FSS_VIM_ACTFIQ / R5FSS_VIM_ACTIRQ), and all interrupts of an equal or lesser priority are masked (discarded). If prior to this interrupt being cleared (by writing to the R5FSS_VIM_FIQVEC register, or R5FSS_VIM_IRQVEC register) another interrupt of higher priority arrives, then the FIQn/IRQn will be asserted and that interrupt made pending as normal. The CPU may or may not service the higher priority interrupt. If the CPU switches this interrupt to active (by reading the R5FSS_VIM_FIQVEC / R5FSS_VIM_IRQVEC register, or (or coreN_IRQACK going high for an IRQ), then the currently active interrupt will be pushed onto a stack. When an interrupt is cleared by writing to the R5FSS_VIM_FIQVEC / R5FSS_VIM_IRQVEC register, if there are any interrupts on the stack, the first entry is popped off and put back into the R5FSS_VIM_ACTFIQ / R5FSS_VIM_ACTIRQ register, so that software may continue where it left off. Note that the R5FSS_VIM_IRQVEC / R5FSS_VIM_FIQVEC address registers are not repopulated with the old vector as it is assumed that the ISR is picking back up where it left off. Only the interrupt number and priority are restored to the R5FSS_VIM_ACTIRQ / R5FSS_VIM_ACTFIQ registers. If software needs the vector again, it will have to read it by using the interrupt number.