SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
For SDRAM data integrity, the MSMC2DDR bridge supports inline ECC on the data written to or read from the SDRAM. ECC is enabled by programming the bits in the DDRSS_ECC_CTRL_REG register. ECC is stored together with the data so that a dedicated SDRAM device for ECC is not required. When using this inline ECC feature the inline ECC inside the DDR controller must be disabled by setting to 0x0 the DDRSS_CTL_206[17-16] ECC_ENABLE field.
8-bit single error correction double error detection (SECDED) ECC is calculated over 64-bit data quanta. For every 512-byte data block 64 bytes of ECC is stored inline. Thus 1/9th of the total SDRAM space is used for ECC storage and the rest 8/9th is available for system use. From system point of view that 8/9th of the SDRAM data space are seen as consecutive byte addresses. Even if there are non-ECC protected regions the previously described 1/9th-8/9th rule still applies and consecutive byte addresses are seen from system point of view.
The ECC is calculated for all accesses that are within the address ranges protected by ECC. The address ranges are specified through the following registers:
The ECC is read and verified during reads if both the DDRSS_ECC_CTRL_REG[0] ECC_EN and DDRSS_ECC_CTRL_REG[2] ECC_CK bits are set to 0x1. For 1-bit ECC error, the MSMC2DDR bridge corrects the data and returns it to the requestor. Although the error is corrected on the returned data, the SDRAM is not corrected. It is responsibility of the system software to correct the ECC error at that location.
It is also responsibility of the system software to pre-load the ECC protected region with known data before functional reads and writes are performed. This can be done by writing to the SDRAM with ECC enabled (DDRSS_ECC_CTRL_REG[0] ECC_EN = 0x1 and DDRSS_ECC_CTRL_REG[1] RMW_EN = 0x1) and ECC check disabled (DDRSS_ECC_CTRL_REG[2] ECC_CK = 0x0). Once the data is loaded in the SDRAM, ECC check must be enabled (DDRSS_ECC_CTRL_REG[2] ECC_CK = 0x1) before using the DDR interface.